NXOpen.UF.ModlFeatures.CreateDatumCsys¶
-
ModlFeatures.
CreateDatumCsys
()¶ Refer to UF_MODL_create_datum_csys for documentation.
Signature:
CreateDatumCsys(objectInPart, xformTag, createComponents)
Parameters: - objectInPart (Tag) – Object in part to define context.
- xformTag (Tag) – Tag of xform object: Must be smart with update option set to SO_update_within_modeling and must be created using one of the construction methods: . defined by three points . defined by two directions and a point . defined by three planes . defined by offset from an existing CSYS
- createComponents (bool) – Flag that if set will create all the components: origin point,3 datum planes and 3 datum axes
Returns: Tag of the datum CSYS feature - If successful
Return type: License requirements: SOLIDS MODELING