NXOpen.UF.ModlFeatures.CreateBridgeFace¶
-
ModlFeatures.
CreateBridgeFace
()¶ Refer to UF_MODL_create_bridge_face for documentation.
Signature:
CreateBridgeFace(continuityType, guideType, primaryFaces, primaryEdges, primaryEdgesDir, sideString1, sideString2, sideFaces, sideEdges)
Parameters: - continuityType (int) – 1 = tangent continuous, 2= curvature continuous
- guideType (int) – 0 = no guides; 1= guide strings; 2= guide surfaces
- primaryFaces (list of Tag) – tags of 2 primary surfaces to be bridged
- primaryEdges (list of Tag) – tags of edges on primary surfaces where the bridge should be attached.
- primaryEdgesDir (int) – direction of primary_edges (if continuity_type = 1) 1 = forward -1 = backward
- sideString1 (
NXOpen.UF.Modl.StringList
Refer to string_list for documentation.) – first guide string (if guide_type = 1) - sideString2 – second guide string (if guide_type = 1)
- sideFaces (list of Tag) – tags of 2 side guide surfaces (if guide_type = 2)
- sideEdges (list of Tag) – tags of edges on side surfaces where bridge should be attached (if guide_type = 2)
Returns: tag of resulting surface
Return type: License requirements: SOLIDS MODELING