NXOpen.UF.ModlFeatures.CreateBplane¶
-
ModlFeatures.
CreateBplane
()¶ Refer to UF_MODL_create_bplane for documentation.
Signature:
CreateBplane(sSection, tol)
Parameters: - sSection (
NXOpen.UF.Modl.StringList
Refer to string_list for documentation.) – Pointer to the curve list structure. int num Total number of curve string loops (min=1, max=150) int string[ ] Total number of segment curves per curve string loop (min=1, max =402) int dir[ ] Direction of a curve string 1 = Start to end -1 = End to start tag_t id[ ] Identifier of section curve - tol (list of float) – Tolerances: [0] = Distance [1] = Angle (in radians) [2] = Not used (formerly listed as Intersection)
Returns: Body object identifier
Return type: License requirements: SOLIDS MODELING
- sSection (