NXOpen.UF.ModlFeatures.AskUGrooveParms¶
-
ModlFeatures.
AskUGrooveParms
()¶ Refer to UF_MODL_ask_u_groove_parms for documentation.
Signature:
AskUGrooveParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier.
- edit (int) – This is an unused flag. It was used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (grooveDia,width,cornerRad)
grooveDia(str): Groove diameter. This must be freed by calling UF_free.
width(str): Groove width. This must be freed by calling UF_free.
cornerRad(str): Groove corner radius. This must be freed by calling UF_free.
License requirements: None