NXOpen.UF.ModlFeatures.AskTaperHoleParms¶
-
ModlFeatures.
AskTaperHoleParms
()¶ Refer to UF_MODL_ask_taper_hole_parms for documentation.
Signature:
AskTaperHoleParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It was used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (diameter,taperAngle,depth,thruFlag)
diameter(str): Hole diameter. This must be freed by calling UF_free.
taperAngle(str): Taper angle. This must be freed by calling UF_free.
depth(str): Hole depth for a none thru hole. This must be freed by calling UF_free.
thruFlag(int): A thru flag can be TRUE or FALSE, if set to TRUE then there is no depth to the hole.
License requirements: None