NXOpen.UF.ModlFeatures.AskRuled¶
-
ModlFeatures.
AskRuled
()¶ Refer to UF_MODL_ask_ruled for documentation.
Signature:
AskRuled(featureObjId)
Parameters: featureObjId (Tag) – Feature object identifier Returns: A Tuple Return type: A tuple consisting of (sSection,sSpine,alignment,value,bodyType,tol) sSection(
`NXOpen.UF.Modl.StringList
Refer to string_list for documentation.`): Pointer to the string list structure for the section strings used to create the feature. Use UF_MODL_free_string_list to deallocate memory.sSpine(
`NXOpen.UF.Modl.StringList
Refer to string_list for documentation.`): Pointer to the string list structure for the spine string. (for alignment = 5). Use UF_MODL_free_string_list to deallocate memory.alignment(int): Alignment method: 1 = Parameter 2 = Arc length 3 = Distance 4 = Angles 5 = Spine curves
value(list of float): Data for alignment method: [0-2] = 3D vector defining direction line (for alignment = 3) [0-5] = 3D start and end coordinates of line defining the axis of revolution for planes (for alignment = 4)
bodyType(int): Type of body: 0 = Sheet 1 = Solid
tol(list of float): Tolerances: [0] = Distance [1] = Angle (in radians)
License requirements: None