NXOpen.UF.ModlFeatures.AskRectPadParms¶
-
ModlFeatures.
AskRectPadParms
()¶ Refer to UF_MODL_ask_rect_pad_parms for documentation.
Signature:
AskRectPadParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It was used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (size,cornerRad,taperAngle)
size(list of str): Pad size (length , width , height).
cornerRad(str): Pad corner radius. This must be freed by calling UF_free.
taperAngle(str): Pad taper angle. This must be freed by calling UF_free.
License requirements: None