NXOpen.UF.ModlFeatures.AskHollowData¶
-
ModlFeatures.
AskHollowData
()¶ Refer to UF_MODL_ask_hollow_data for documentation.
Signature:
AskHollowData(featureId, type)
Parameters: - featureId (Tag) – Feature identifier
- type (int) – Hollow type:1 = face 2 = region 3 = body
Returns: A Tuple
Return type: A tuple consisting of (tolerance,thickness,nPiercedFaces,piercedFaces,nBoundaryFaces,boundaryFaces,nOffsetFaces,offsetFaces,offsetThickness)
tolerance(float): Tolerance.
thickness(str): Default thickness. This must be freed bycalling UF_free.
nPiercedFaces(int): Number of pierced faces
piercedFaces(list of Tag): n_pierced_facesArray of pierced face identifiers. This array must be freed by calling UF_free.
nBoundaryFaces(int): Number of boundary faces
boundaryFaces(list of Tag): n_boundary_facesArray of boundary face identifers. This array must be freed by calling UF_free.
nOffsetFaces(int): Number of offset faces
offsetFaces(list of Tag): n_offset_facesArray of offset face ids. This array must be freed by calling UF_free.
offsetThickness(list of str): n_offset_facesArray of offset thickness expressions. This array must be freed by calling UF_free_string_array.
License requirements: None