NXOpen.UF.ModlFeatures.AskCurveMesh¶
-
ModlFeatures.
AskCurveMesh
()¶ Refer to UF_MODL_ask_curve_mesh for documentation.
Signature:
AskCurveMesh(featureObjId)
Parameters: featureObjId (Tag) – Feature object identifier Returns: A Tuple Return type: A tuple consisting of (sPrim,sCross,sSpine,emphasis,bodyType,splinePts,tol,cFaceId,cFlag) sPrim(
`NXOpen.UF.Modl.StringList
Refer to string_list for documentation.`): Pointer to the string list structu re, containing the data defining the primary curves used to create the feature. See structure section of manual for details. Use UF_MODL_free_string_list to deallocate memory.sCross(
`NXOpen.UF.Modl.StringList
Refer to string_list for documentation.`): Pointer to the string list structure, containing the data defining the cross curves used to create the feature. See structure section of manual for details. Use UF_MODL_free_string_list to deallocate memory.sSpine(
`NXOpen.UF.Modl.StringList
Refer to string_list for documentation.`): Pointer to the string list structure for the spine string. See structure section of manual for details. Use UF_MODL_free_string_list to deallocate memory.emphasis(int): Emphasis flag 1 = Primary curves 2 = Cross curves 3 = Both
bodyType(int): Type of body: 0 = Sheet 1 = Solid
splinePts(int): Spline points flag: 0 = Do not reparameterize curves 1 = Reparameterize through spline points
tol(list of float): Tolerances: [0] = Distance [1] = Angle (in degrees) [2] = Intersection
cFaceId(list of Tag): Object identifiers of neighbor surfaces from which constraints are obtained [0] = first primary string [1] = last primary string [2] = first cross string [3] = last cross string No constraint is imposed on the corresponding string if id = NULL_TAG
cFlag(list of int): [0] = first primary string constraint type [1] = last primary string constraint type [2] = first cross string constraint type [3] = last cross string constraint type The constraint types are as follows: 0 = no constraint 1 = tangency constraint 2 = curvature constraint
License requirements: None