NXOpen.UF.ModlFeatures.AskBossParms¶
-
ModlFeatures.
AskBossParms
()¶ Refer to UF_MODL_ask_boss_parms for documentation.
Signature:
AskBossParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (diameter,height,taperAngle)
diameter(str): Boss diameter. This must be freed by calling UF_free.
height(str): Boss height. This must be freed by calling UF_free.
taperAngle(str): Boss taper angle. This must be freed by calling UF_free.
License requirements: None