NXOpen.UF.ModlFeatures.AskBlockParms¶
-
ModlFeatures.
AskBlockParms
()¶ Refer to UF_MODL_ask_block_parms for documentation.
Signature:
AskBlockParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: Block dimension (length , width , height) The string space allocated for the three elements should be freed via UF_free when they are not used.
Return type: list of str
License requirements: None