NXOpen.UF.ModlFeatures.AskBlendParms¶
-
ModlFeatures.
AskBlendParms
()¶ Refer to UF_MODL_ask_blend_parms for documentation.
Signature:
AskBlendParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: Blend radius. This must be freed by calling UF_free.
Return type: str
License requirements: None