NXOpen.UF.Modl.Faces Structure¶
NXOpen.UF.Modl.Faces is an alias for NXOpen.UF.ModlFaces_Struct
-
class
NXOpen.UF.
ModlFaces_Struct
¶ Bases:
object
Refer to UF_MODL_faces_s for documentation.
Fields
NXOpen.UF.ModlFaces_Struct.NumberOfFaces |
Number of faces supplied in the following array. |
NXOpen.UF.ModlFaces_Struct.Faces |
Array of faces to be used in the function. |
NXOpen.UF.ModlFaces_Struct.FaceExtension |
Indication of how the faces should be extended if the function allows for face extension. |