NXOpen.UF.Modl.EdgeBlendSetbackData Structure¶
NXOpen.UF.Modl.EdgeBlendSetbackData is an alias for NXOpen.UF.ModlEdgeBlendSetbackData_Struct
-
class
NXOpen.UF.
ModlEdgeBlendSetbackData_Struct
¶ Bases:
object
Refer to UF_MODL_edge_blend_setback_data_s for documentation.
Fields
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.Edge |
The edge on which setback distance has to be specified |
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.FromStart |
if true, then the setback is defined at the start vertex. Otherwise, it is defined at the end vertex. |
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.Distance |
Setback distance |
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.DistanceExp |
Expression TAG will only be set during Edit, User can edit the distance string to edit the new value |
NXOpen.UF.ModlEdgeBlendSetbackData_Struct.Status |
When adding Status = 1 and To remove Status = 0 |