NXOpen.UF.Modl.EdgeBlendSet Structure¶
NXOpen.UF.Modl.EdgeBlendSet is an alias for NXOpen.UF.ModlEdgeBlendSet_Struct
-
class
NXOpen.UF.
ModlEdgeBlendSet_Struct
¶ Bases:
object
Refer to UF_MODL_edge_blend_set_s for documentation.
Fields
NXOpen.UF.ModlEdgeBlendSet_Struct.EdgeCollector |
The edge collector, if this is a NULL_TAG, then the edges will be read from num_edges and edges |
NXOpen.UF.ModlEdgeBlendSet_Struct.NumEdges |
The edges with a constant radius. |
NXOpen.UF.ModlEdgeBlendSet_Struct.Edges |
|
NXOpen.UF.ModlEdgeBlendSet_Struct.Radius |
Radius associated with these edges |
NXOpen.UF.ModlEdgeBlendSet_Struct.RadiusExp |
Expression TAG will only be set during Edit, User can edit the radius string to edit the new value |
NXOpen.UF.ModlEdgeBlendSet_Struct.Status |
When adding Status = 1 and To remove Status = 0 |