NXOpen.UF.Modl.DevchkEeInfo Structure¶
NXOpen.UF.Modl.DevchkEeInfo is an alias for NXOpen.UF.ModlDevchkEeInfo_Struct
-
class
NXOpen.UF.
ModlDevchkEeInfo_Struct
¶ Bases:
object
Refer to UF_MODL_devchk_ee_info_s for documentation.
Fields
NXOpen.UF.ModlDevchkEeInfo_Struct.DevType |
0 - no deviation1 - step 2 - overlap 3 - gap |
NXOpen.UF.ModlDevchkEeInfo_Struct.Face1Tag |
face tag on which edge_1_pnt lies |
NXOpen.UF.ModlDevchkEeInfo_Struct.Edge1Pnt |
point on an edge of face_pairs[0] used for deviation checking |
NXOpen.UF.ModlDevchkEeInfo_Struct.Norm1 |
face normal at edge_1_pnt |
NXOpen.UF.ModlDevchkEeInfo_Struct.Face2Tag |
face tag on which edge_2_pnt lies |
NXOpen.UF.ModlDevchkEeInfo_Struct.Edge2Pnt |
point on an edge of face_pairs[1], where the minimum deviation occured from edge_1_pnt |
NXOpen.UF.ModlDevchkEeInfo_Struct.Norm2 |
face normal at edge_2_pnt |
NXOpen.UF.ModlDevchkEeInfo_Struct.EdgeDist |
distance between edge_1_pnt and edge_2_pnt |
NXOpen.UF.ModlDevchkEeInfo_Struct.NormAngle |
Angle between the face normals |