NXOpen.UF.Modl.BlendFacesLimitData Structure¶
NXOpen.UF.Modl.BlendFacesLimitData is an alias for NXOpen.UF.ModlBlendFacesLimitData_Struct
-
class
NXOpen.UF.
ModlBlendFacesLimitData_Struct
¶ Bases:
object
Refer to UF_MODL_blend_faces_limit_data_s for documentation.
Fields
NXOpen.UF.ModlBlendFacesLimitData_Struct.UseStartLimit |
If TRUE, the blend is trimmed to start in a constant parameter line determined by a start limiting plane. |
NXOpen.UF.ModlBlendFacesLimitData_Struct.StartLimit |
Definition of the start limit plane (point and a normal vector). |
NXOpen.UF.ModlBlendFacesLimitData_Struct.UseEndLimit |
If TRUE, the blend is trimmed to end in a constant parameter line determined by a start limiting plane. |
NXOpen.UF.ModlBlendFacesLimitData_Struct.EndLimit |
Definition of the end limit plane (point and a normal vector). |
NXOpen.UF.ModlBlendFacesLimitData_Struct.UseHelpPoint |
If TRUE, use a help point to differentiate between multiple alternative possible blends between the faces. |
NXOpen.UF.ModlBlendFacesLimitData_Struct.HelpPoint |
Coordinates of the help point. |