NXOpen.UF.Modl.IdentifyExteriorUsingHl¶
-
Modl.
IdentifyExteriorUsingHl
()¶ Refer to UF_MODL_identify_exterior_using_hl for documentation.
Signature:
IdentifyExteriorUsingHl(numBodies, bodies, xforms, numDirs, direction, chordalTol, resolution, numFaces)
Parameters: - numBodies (int) – Number of tags in the bodies array.
- bodies (list of Tag) – Array of body tags to identify faces from.
- xforms (list of Tag) – Array of xforms. One for each body, determines the position of the body relative to its source geometry. NULL_TAG implies no transformation.
- numDirs (int) – Number of directions
- direction (list of float) – Direction to apply hidden line solution from
- chordalTol (float) – Chordal tolerance for edges
- resolution (int) – Determines how many hatch lines drawnper face. May be one of: UF_LINKED_HL_RES_COARSE UF_LINKED_HL_RES_NORMAL UF_LINKED_HL_RES_FINE UF_LINKED_HL_RES_VERY_FINE
- numFaces (int) – Number of tags in the faces array.If input is > 0 will reallocate and add external faces to existing output arrays
Returns: A Tuple
Return type: A tuple consisting of (numFaces,faces,bodyIndex)
numFaces(int): Modified value of numFaces
faces(list of Tag): Array of face tags.
bodyIndex(list of int): Array of indices giving the body/xform the face came from.
License requirements: SOLIDS MODELING