NXOpen.UF.Modl.CreateRevolution¶
-
Modl.
CreateRevolution
()¶ Refer to UF_MODL_create_revolution for documentation.
Signature:
CreateRevolution(objects, objectArg, trimData, limit, offsets, regionPoint, regionSpecified, solidCreation, axisPoint, direction, sign)
Parameters: - objects (list of Tag) – Array of objects or one section builder object tag but not both, to be revolved
- objectArg (int) – Count of objects
- trimData (
NXOpen.UF.Modl.SweepTrimObject
Refer to UF_MODL_SWEEP_TRIM_object_s for documentation.) – Pointer to structure for trimming data - limit (list of str) – Limit of revolution.
- offsets (list of str) – Offsets for open strings
- regionPoint (list of float) – Point on region of object
- regionSpecified (bool) – True or False for region desired
- solidCreation (bool) – If the body_type preference set by UF_MODL_set_body_type_pref is UF_MODL_SOLID_BODY, and solid_creation is set to TRUE, then UF_MODL_create_revolution creates solid bodies if the input string is closed. Otherwise, sheet bodies are the result.
- axisPoint (list of float) – Point of origin for axis direction vector
- direction (list of float) – Revolution axis direction vector.
- sign (
NXOpen.UF.Modl.FeatureSigns
Refer to UF_FEATURE_SIGNS for documentation.) – The sign of the operation to be performed. UF_NULLSIGN = create new target solid UF_POSITIVE = add to target solid UF_NEGATIVE = subtract from target solid UF_UNSIGNED = intersect with target solid
Returns: A Tuple
Return type: A tuple consisting of (features,numberOfFeatures)
features(list of Tag): Array of revolved feature tags. This must be freed by calling UF_free.
numberOfFeatures(int): Number of features returned
License requirements: SOLIDS MODELING