NXOpen.UF.Modl.CreateExtrusionPath¶
-
Modl.
CreateExtrusionPath
()¶ Refer to UF_MODL_create_extrusion_path for documentation.
Signature:
CreateExtrusionPath(objects, objectCount, pathObjects, path, trimData, offsets, regionPoint, regionSpecified, solidCreation, sign)
Parameters: - objects (list of Tag) – Section Objects.
- objectCount (int) – Number of section objects
- pathObjects (list of Tag) – Path objects
- path (int) – Number of path objects
- trimData (
NXOpen.UF.Modl.SweepTrimObject
Refer to UF_MODL_SWEEP_TRIM_object_s for documentation.) – Not used - offsets (list of str) – Offsets
- regionPoint (list of float) – Point in desired region
- regionSpecified (bool) – True or False for region desired
- solidCreation (bool) – If TRUE, create solid bodies if input string closed. Otherwise, sheet bodies are the result.
- sign (
NXOpen.UF.Modl.FeatureSigns
Refer to UF_FEATURE_SIGNS for documentation.) – The sign of the operation to be performed. UF_NULLSIGN = create new target solid UF_POSITIVE = add to target solid UF_NEGATIVE = subtract from target solid UF_UNSIGNED = intersect with target solid
Returns: A Tuple
Return type: A tuple consisting of (features,numberOfFeatures)
features(list of Tag): Array of extrude feature tags. This must be freed by calling UF_free.
numberOfFeatures(int): Number of features returned
License requirements: SOLIDS MODELING