NXOpen.UF.Modl.CreateExtruded¶
-
Modl.
CreateExtruded
()¶ Refer to UF_MODL_create_extruded for documentation.
Signature:
CreateExtruded(objects, taperAngle, limit, point, direction, sign)
Parameters: - objects (
NXOpen.UF.UF.List
Refer to ` <../ugopen_doc/uf/.html>`_ for documentation.) – List of objects to be extruded. - taperAngle (str) – Taper angle (in degrees).
- limit (list of str) – Limit of extrusion. This is declared as: char *limit[2]. The first value is the start value of the extrusion and the second value is the end of the extrusion (see the example program).
- point (list of float) – not used
- direction (list of float) – Extrusion axis.
- sign (
NXOpen.UF.Modl.FeatureSigns
Refer to UF_FEATURE_SIGNS for documentation.) – The sign of the operation to be performed. UF_NULLSIGN = create new target solid UF_POSITIVE = add to target solid UF_NEGATIVE = subtract from target solid UF_UNSIGNED = intersect with target solid
Returns: List of feature identifiers created. This list must be freed by calling UF_MODL_delete_list.
Return type: NXOpen.UF.UF.List
Refer to ` <../ugopen_doc/uf/.html>`_ for documentation.License requirements: SOLIDS MODELING
- objects (