NXOpen.UF.Modl.AskTSlotParms¶
-
Modl.
AskTSlotParms
()¶ Refer to UF_MODL_ask_t_slot_parms for documentation.
Signature:
AskTSlotParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier.
- edit (int) – This is an unused flag. It was used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (topWidth,topDepth,bottomWidth,bottomDepth,distance,thruFlag)
topWidth(str): Slot top width. This must be freed by calling UF_free.
topDepth(str): Slot top depth. This must be freed by calling UF_free.
bottomWidth(str): Slot bottom width. This must be freed by calling UF_free.
bottomDepth(str): Slot bottom depth. This must be freed by calling UF_free.
distance(str): Slot distance for a none thru slot. This must be freed by calling UF_free.
thruFlag(int): A thru flag can be TRUE or FALSE, if set to TRUE then there is no distance to the slot.
License requirements: None