NXOpen.UF.Modl.AskSweepParms¶
-
Modl.
AskSweepParms
()¶ Refer to UF_MODL_ask_sweep_parms for documentation.
Signature:
AskSweepParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It was used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (taperAngle,limit1,limit2)
taperAngle(str): Taper angle. This must be freed by calling UF_free.
limit1(str): Start angle (degrees) for revolved features or start offset distance for extruded features. This must be freed by calling UF_free.
limit2(str): End angle (degrees) for revolved features or end offset distance for extruded features. This must be freed by calling UF_free.
License requirements: None