NXOpen.UF.Modl.AskRectSlotParms¶
-
Modl.
AskRectSlotParms
()¶ Refer to UF_MODL_ask_rect_slot_parms for documentation.
Signature:
AskRectSlotParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It was used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (width,depth,distance,thruFlag)
width(str): Slot width. This must be freed by calling UF_free.
depth(str): Slot depth. This must be freed by calling UF_free.
distance(str): Slot distance for a none thru slot. This must be freed by calling UF_free.
thruFlag(int): A thru flag can be TRUE or FALSE, if set to TRUE then there is no distance to the slot.
License requirements: None