NXOpen.UF.Modeling.TrimSheet¶
-
Modeling.
TrimSheet
()¶ Refer to UF_MODL_trim_sheet for documentation.
Signature:
TrimSheet(sheetBodyTag, countBoundingObjects, boundingObjects, projectionVector, pointKey, pointCount, pointCoords, tolerance)
Parameters: - sheetBodyTag (Tag) – Tag of sheet body to trim.
- countBoundingObjects (int) – Number of trimming objects.
- boundingObjects (list of
NXOpen.UF.Modl.TrimObject
Refer to UF_MODL_trim_object for documentation.) – Array of pointers to structures holding trimming object data. - projectionVector (list of float) – Vector for curves projected along a vector.
- pointKey (int) – Points define regions to: 0 = discard 1 = keep
- pointCount (int) – Number of points. (Number of regions.)
- pointCoords (list of float) – Array of points on the sheet. (3 * point_count values.)
- tolerance (float) – Distance tolerance for any approximations.
Returns: A Tuple
Return type: A tuple consisting of (numberGapPoints,gapPoints)
numberGapPoints(int): Number of points returned in gap_points.
gapPoints(list of float): Array of points showing positions of gaps. (3 * number_gap_points values.) This array must be freed by calling UF_free.
License requirements: SOLIDS MODELING