NXOpen.UF.Modeling.SetFeatTolerance¶
-
Modeling.
SetFeatTolerance
()¶ Refer to UF_MODL_set_feat_tolerance for documentation.
Signature:
SetFeatTolerance(featureObjId, tolerance, updatePart)
Parameters: - featureObjId (Tag) – Feature to set
- tolerance (float) – Distance tolerance to set in the feature
- updatePart (bool) – Indicate whether to update the part.If TRUE - Part will get updated by calling UF_MODL_update, FALSE - Part will not get updated, User has to update the part. User can set the tolerance of multiple features and then update the part by calling UF_MODL_update at end or pass the update_part flag as true for last feature
License requirements: None