NXOpen.UF.Modeling.IsBrowseableFeature¶
-
Modeling.
IsBrowseableFeature
()¶ Refer to UF_MODL_is_browseable_feature for documentation.
Signature:
IsBrowseableFeature(featureTag, reportInactiveFeature, reportFeatureUnableToMakeCurrent)
Parameters: - featureTag (Tag) – The feature whose browseable status is to be checked.
- reportInactiveFeature (bool) – TRUE: Inactive feature is reported as browseable. FALSE: Inactive feature is not reported as browseable.
- reportFeatureUnableToMakeCurrent (bool) – TRUE: Feature that cannot be made current is reported as browseable. FALSE: Feature that cannot be made current is not reported as browseable.
Returns: True if the feature is browseable, false otherwise.
Return type: bool
License requirements: None