NXOpen.UF.Modeling.IntersectCurveToPlane¶
-
Modeling.
IntersectCurveToPlane
()¶ Refer to UF_MODL_intersect_curve_to_plane for documentation.
Signature:
IntersectCurveToPlane(curveId, planeId)
Parameters: Returns: A Tuple
Return type: A tuple consisting of (numIntersections,data)
numIntersections(int): number of intersections
data(list of float): This array must be freed by calling UF_free. It is a one dimensional array whose size is num_intersections * 4 data[4*i + 0], data[4*i + 1] and data[4*i + 2] holds the coordinates of the point data[4*i + 3] holds the parameter of first curve or edge
License requirements: SOLIDS MODELING