NXOpen.UF.Modeling.IntersectCurveToFace¶
-
Modeling.
IntersectCurveToFace
()¶ Refer to UF_MODL_intersect_curve_to_face for documentation.
Signature:
IntersectCurveToFace(curveId, faceId)
Parameters: Returns: A Tuple
Return type: A tuple consisting of (numIntersections,data)
numIntersections(int): number of intersections
data(list of float): This array must be freed by calling UF_free. It is a one dimensional array whose size is num_intersections * 6 data[6*i + 0], data[6*i + 1] and data[6*i + 2] holds the coordinates of the point data[6*i + 3] holds the parameter of first curve or edge data[6*i + 4] holds the u parameter of face data[6*i + 5] holds the v parameter of face
License requirements: SOLIDS MODELING