NXOpen.UF.Modeling.DevchkAdjacentEdges¶
-
Modeling.
DevchkAdjacentEdges
()¶ Refer to UF_MODL_devchk_adjacent_edges for documentation.
Signature:
DevchkAdjacentEdges(numFaces, faces, tolerances, numChkPoints)
Parameters: - numFaces (int) – Number of input faces for deviation checking
- faces (list of Tag) – Array of face tags to be checked.
- tolerances (float) – [0] - Common Edge Tolerance: Edges with maximum distance greater than this value are non-common edges [1] - Chordal Deviation: Used for sampling the edges if num_chk_points is zero.
- numChkPoints (int) – if non-zero, edges are sampled at equallyspaced parameter values. if zero, Chordal Deviation is used for sampling.
Returns: A Tuple
Return type: A tuple consisting of (numDevs,devs)
numDevs(int): Number of deviations returned.
devs(list of ``NXOpen.UF.Modl.DevchkEeInfo` Refer to UF_MODL_devchk_ee_info_s for documentation.`): deviations information correspondingto each sample point. The caller is responsible for calling UF_free to free this array.
License requirements: SOLIDS MODELING