NXOpen.UF.Modeling.CreateSubdivFace¶
-
Modeling.
CreateSubdivFace
()¶ Refer to UF_MODL_create_subdiv_face for documentation.
Signature:
CreateSubdivFace(curveRefs, count, face, projType, vector)
Parameters: - curveRefs (list of Tag) – Array of curves to subdivide the face with
- count (int) – Number of curves in curve_refs
- face (Tag) – Face object identifier
- projType (int) – Projection type 1 = Along surface normal 2 = Along vector (Not implemented yet)
- vector (list of float) – Projection vector if projection type = 2 (Not used)
Returns: Feature object identifier of created subdivide face
Return type: License requirements: SOLIDS MODELING