NXOpen.UF.Modeling.CreateSew¶
-
Modeling.
CreateSew
()¶ Refer to UF_MODL_create_sew for documentation.
Signature:
CreateSew(option, numTargets, targets, numTools, tools, tolerance, typeBody)
Parameters: - option (int) – Option flag: 0 = Sew general 1 = Sew all instances
- numTargets (int) – Size of the targets array
- targets (list of Tag) – Array of target tags ( sheet body when type_body = 0 or face(s) from a solid body when type_body = 1 ).
- numTools (int) – Size of the tool array
- tools (list of Tag) – Array of tool tags ( sheet body when type_body = 0 or face(s) from a solid body when type_body = 1 ).
- tolerance (float) – Tolerance value
- typeBody (int) – Type of body: 0 = Sheet (default) 1 = Solid
Returns: A Tuple
Return type: A tuple consisting of (disjointList,sewId)
disjointList(
`NXOpen.UF.UF.List
Refer to ` <../ugopen_doc/uf/.html>`_ for documentation.`): List contains disjoint sheets from the target. This list must be freed by calling UF_MODL_delete_list.sewId(Tag): The sew feature that was created.
License requirements: SOLIDS MODELING