NXOpen.UF.Modeling.CreateReverseNormal¶
-
Modeling.
CreateReverseNormal
()¶ Refer to UF_MODL_create_reverse_normal for documentation.
Signature:
CreateReverseNormal(sheetBodyTag, optionFlag)
Parameters: - sheetBodyTag (Tag) – sheet body to be reversed
- optionFlag (int) – = 0 - do not allow multiple reverse normal features on the sheet body = 1 - allow multiple reverse normal features on the sheet body
Returns: identifier for reverse normal feature
Return type: License requirements: SOLIDS MODELING