NXOpen.UF.Modeling.CreateFaceOffset¶
-
Modeling.
CreateFaceOffset
()¶ Refer to UF_MODL_create_face_offset for documentation.
Signature:
CreateFaceOffset(offset, faces)
Parameters: - offset (str) – Offset offset. Value must be greater than 1e-6 otherwise it is regarded as zero which is an invalid input. We do not support zero as input.
- faces (
NXOpen.UF.UF.List
Refer to ` <../ugopen_doc/uf/.html>`_ for documentation.) – Offset feature/face object list. You can input a face collector tag in the list. If you input a face collector, the face collector should be the only member in the list.
Returns: Feature object identifier of created face offset
Return type: License requirements: SOLIDS MODELING