NXOpen.UF.Modeling.CompareTopology¶
-
Modeling.
CompareTopology
()¶ Refer to UF_MODL_compare_topology for documentation.
Signature:
CompareTopology(solidObject1, solidObject2, facetTolerance, distanceTolerance)
Parameters: - solidObject1 (Tag) – Object identifier of first object (valid objects are faces and edges)
- solidObject2 (Tag) – Object identifier of second object (valid objects are faces and edges)
- facetTolerance (float) – Specifies the maximum distance any point on a facet can be from its parent surface. All vertices of facets are on the surface.
- distanceTolerance (float) – Specifies the maximum distance a vertex of a facet can be from the other surface.
Returns: Status value: COMPARE_NOMATCH COMPARE_FACES_IDENTICAL COMPARE_FACES_EQUIVALENT COMPARE_SURFACES_IDENTICAL COMPARE_SURFACES_EQUIVALENT COMPARE_EDGES_IDENTICAL COMPARE_EDGES_EQUIVALENT COMPARE_CURVES_IDENTICAL COMPARE_CURVES_EQUIVALENT Descriptions for these values are given in a table which follows in the general function description.
Return type: int
License requirements: SOLIDS MODELING