NXOpen.UF.Modeling.AskSubdivFaceParms¶
-
Modeling.
AskSubdivFaceParms
()¶ Refer to UF_MODL_ask_subdiv_face_parms for documentation.
Signature:
AskSubdivFaceParms(featureObjId)
Parameters: featureObjId (Tag) – Feature object identifier of a subdivided face Returns: A Tuple Return type: A tuple consisting of (face,curves,count,projType,vector) face(Tag): Face object identifier which the subdivided face is on
curves(list of Tag): Pointer to array of curves associated with the subdivide face feature
count(int): Number of curves in curve array
projType(int): Projection type 1 = Along surface normal 2 = Along vector (Not implemented yet)
vector(float): Projection vector (Not used)
License requirements: None