NXOpen.UF.Modeling.AskPerpDist¶
-
Modeling.
AskPerpDist
()¶ Refer to UF_MODL_ask_perp_dist for documentation.
Signature:
AskPerpDist(feature, constraint, edit)
Parameters: Returns: A Tuple
Return type: A tuple consisting of (fixed1,fixed2,feature1,feac,howFar,tool,part)
fixed1(list of float): Dimension attachment point on the part.
fixed2(list of float): Point on the part that along with the fixed1 point, defines the line that the dimension is perpendicular to.
feature1(list of float): Dimension attachment point on the part.
feac(list of float): Center of arc if the attachment point is tangent to arc edge of feature, otherwise it is the same as the feature point.
howFar(str): Expression distance. This must be freed by calling UF_free.
tool(Tag): Edge on the tool or NULL_TAG for a centerline
part(Tag): Edge on the part
License requirements: None