NXOpen.UF.Modeling.AskParaEdge¶
-
Modeling.
AskParaEdge
()¶ Refer to UF_MODL_ask_para_edge for documentation.
Signature:
AskParaEdge(featureObjId, constraint, edit)
Parameters: Returns: A Tuple
Return type: A tuple consisting of (fixed1,fixed2,feature1,feature2,parallel,howFar,tool,part)
fixed1(list of float): Dimension attachment point on the part
fixed2(list of float): Point on the part that along with the fixed1 point, defines the line on the part that the dimension is parallel to.
feature1(list of float): Dimension attachment point on the feature.
feature2(list of float): Point on the feature that along with the feature1 point, defines the line on the feature that the dimension is parallel to.
parallel(int): Is this a parallel constraint or a perpendicular constraint? TRUE=Parallel, FALSE=perpendicular
howFar(str): Expression distance. This must be freed by calling UF_free.
tool(Tag): Edge on the tool or NULL_TAG for a centerline.
part(Tag): Edge on the part
License requirements: None