NXOpen.UF.Modeling.AskParaDist¶
-
Modeling.
AskParaDist
()¶ Refer to UF_MODL_ask_para_dist for documentation.
Signature:
AskParaDist(featureObjId, constraint, edit)
Parameters: Returns: A Tuple
Return type: A tuple consisting of (fixed,feature,fixc,feac,howFar,tool,part)
fixed(list of float): Dimension attachment point on the part
feature(list of float): Dimension attachment point on the feature
fixc(list of float): Center of arc if attachment point is tangent to arc edge on part, otherwise it is the same as the fixed point.
feac(list of float): Center of arc if attachment point is tangent to arc edge on feature, otherwise it is the same as the feature point.
howFar(str): Expression distance. This must be freed by the caller by calling UF_free.
tool(Tag): Edge on the tool or NULL_TAG for a centerline
part(Tag): Edge on the part
License requirements: None