NXOpen.UF.Modeling.AskFaceTopology¶
-
Modeling.
AskFaceTopology
()¶ Refer to UF_MODL_ask_face_topology for documentation.
Signature:
AskFaceTopology(faceId)
Parameters: faceId (Tag) – Object identifier for the face Returns: Topological type of a face: UF_MODL_FLAT_TOPOLOGY = 1 peripheral loop UF_MODL_CYLINDRICAL_TOPOLOGY = 2 peripheral loops, no pole UF_MODL_CONICAL_TOPOLOGY = 2 peripheral loops, 1 pole UF_MODL_SPHERICAL_TOPOLOGY = 2 peripheral loops, 2 poles UF_MODL_TOROIDAL_TOPOLOGY = no peripheral loops 0 = if error, or if input was a body with multiple faces Return type: int License requirements: None