NXOpen.UF.Modeling.AskFaceSelfIntersect¶
-
Modeling.
AskFaceSelfIntersect
()¶ Refer to UF_MODL_ask_face_self_intersect for documentation.
Signature:
AskFaceSelfIntersect(faceTag)
Parameters: faceTag (Tag) – face tag Returns: A Tuple Return type: A tuple consisting of (faultToken,point) faultToken(int): Fault token. If 0, then the face is not self-intersecting. Otherwise it is a model error code that can be converted to a string by calling UF_get_fail_message.
point(list of float): Point of self-intersection in ABS coordinates
License requirements: None