NXOpen.UF.Modeling.AskChamferParms¶
-
Modeling.
AskChamferParms
()¶ Refer to UF_MODL_ask_chamfer_parms for documentation.
Signature:
AskChamferParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (subtype,radius1,radius2,theta)
subtype(int): Chamfer subtype 1 = Single offset. 2 = Double offsets. 3 = Offset and angle. 4 = Freeform Single Offset 5 = Freeform Double Offset
radius1(str): Chamfer offset. This must be freed by calling UF_free.
radius2(str): Chamfer offset not valid for subtype 1 and 3. This must be freed by calling UF_free.
theta(str): Chamfer angle not valid for subtype 1 and 2. This must be freed by calling UF_free.
License requirements: None