NXOpen.UF.Modeling.AskBooleanWithRetainedOptions¶
-
Modeling.
AskBooleanWithRetainedOptions
()¶ Refer to UF_MODL_ask_boolean_with_retained_options for documentation.
Signature:
AskBooleanWithRetainedOptions(featureEid)
Parameters: featureEid (Tag) – Boolean feature Returns: A Tuple Return type: A tuple consisting of (sign,originalTarget,originalTool,retainTargetBody,retainToolBody) sign(
`NXOpen.UF.Modl.FeatureSigns
Refer to UF_FEATURE_SIGNS for documentation.`): Type of boolean:* - UF_POSITIVE : unite * - UF_NEGATIVE : subtract * - UF_UNSIGNED : intersectoriginalTarget(Tag): Original target body
originalTool(Tag): Original tool body
retainTargetBody(bool): Indicate whether to retain the target body. If TRUE - the resulting body is the new body and target body is retained, FALSE - the resulting body is the modified target body.
retainToolBody(bool): Indicate whether to retain the tool body.If TRUE - the tool body is not consumed. FALSE - the tool body is consumed
License requirements: None