NXOpen.UF.Modeling.AskBodyConsistency¶
-
Modeling.
AskBodyConsistency
()¶ Refer to UF_MODL_ask_body_consistency for documentation.
Signature:
AskBodyConsistency(bodyTag)
Parameters: bodyTag (Tag) – body tag Returns: A Tuple Return type: A tuple consisting of (numTags,faultTokens,faultTags) numTags(int): The number of faces/edges in the input body which don’t pass the consistency check.
faultTokens(list of int): Array of fault tokens. Each token is a UF_MODL error code, which can be translated to a string by passing it to UF_get_fail_message. This array must be freed by calling UF_free.
faultTags(list of Tag): Array of tags of faces/edges which don’t pass the consistency check This array must be freed by calling UF_free.
License requirements: None