NXOpen.UF.Mct.ReplaceMachine¶
-
Mct.
ReplaceMachine
()¶ Refer to UF_MCT_replace_machine for documentation.
Signature:
ReplaceMachine(libref, retrieveOpt, mountingOpt)
Parameters: - libref (str) –
- the library reference of the desired* machine tool. Can be gotten from a record * set or an existing NX object
- retrieveOpt (int) –
- Flag indicating whether tool pocket datais to be retrieved with new machine: 0 = No 1 = Yes
- mountingOpt (
NXOpen.UF.Lib.NcmctSetupReplaceMode
Refer to UF_NCMCT_setup_replace_mode_t for documentation.) –- Flag indicating how the machine is to belocated with respect to the part if there is a part file associated with the machine: 0 = No mounting. Machine is loaded as defined. 1 = Mount the machine onto the workpiece. 2 = Mount the workpiece onto the machine.
Returns: - the NX object created as a result of the* retrieval
Return type: License requirements: None
- libref (str) –