NXOpen.UF.Layer.CycleByLayer¶
-
Layer.
CycleByLayer
()¶ Refer to UF_LAYER_cycle_by_layer for documentation.
Signature:
CycleByLayer(layerNumber, objectTag)
Parameters: - layerNumber (int) – Layer number to cycle, pass in a layer number of 0 to cycle all enabled layers.
- objectTag (Tag) – On input the object found by the last call to this routine. Begin the cycle by passing in object = NULL_TAG On output, the next object on the specified layer or layers. Outputs a NULL_TAG when the cycle is finished.
Returns: Modified value of objectTag
Return type: License requirements: None