NXOpen.UF.Kf.CreateChildRule¶
-
Kf.
CreateChildRule
()¶ Refer to UF_KF_create_child_rule for documentation.
Signature:
CreateChildRule(partOfRule, nameChain, ruleName, childClassName, numParameters, parameterNames, parameterRules)
Parameters: - partOfRule (Tag) – Part to create or modify rule in
- nameChain (str) – Reference chain of instance, with trailing colon, where rule will be created or modified. If create then must be “Root:” or NULL. Child rules can only be created on the “Root:”
- ruleName (str) – Name of rule.
- childClassName (str) – Class of instance
- numParameters (int) – number of parameters in the parameter_names array
- parameterNames (list of str) – num_parametersarray of names of parameters specified by the user.
- parameterRules (list of str) – num_parametersarray of rules for the parameters whose names are in “parameter_names” above. Each rule may or may not have a trailing semicolon.
Returns: name generated for the child object.Currently always returns NULL.
Return type: str
License requirements: None