NXOpen.UF.Gexp.EditDistance¶
-
Gexp.
EditDistance
()¶ Refer to UF_GEXP_edit_distance for documentation.
Signature:
EditDistance(featureTag, newFromObject, newXform1, newToObject, newXform2)
Parameters: - featureTag (Tag) – Tag of distance expression feature to edit.
- newFromObject (Tag) – Tag of object to use for newly edited distance. Occurrence tags are not allowed. Use the prototype tag instead.
- newXform1 (Tag) – Tag of transformation for first object. This tag is NULL_TAG if the object is in the same part in which the feature is created.
- newToObject (Tag) – Tag of object to use for newly edited distance. Occurrence tags are not allowed. Use the prototype tag instead.
- newXform2 (Tag) – Tag of transformation for second object. This tag is NULL_TAG if the object is in the same part in which the feature is created.
License requirements: None