NXOpen.UF.Gexp.CreateLength¶
-
Gexp.
CreateLength
()¶ Refer to UF_GEXP_create_length for documentation.
Signature:
CreateLength(objectArg, xform)
Parameters: - objectArg (Tag) – Tag of object for which to create the length. Valid object types are: UF_line_type UF_circle_type UF_spline_type UF_conic_type UF_solid_type Occurrence tags are not allowed. Use the prototype tag instead.
- xform (Tag) – Tag of transformation for the object. The tag is NULL_TAG if the object is in the same part in which the feature is created.
Returns: A Tuple
Return type: A tuple consisting of (featureTag,expTag)
featureTag(Tag): Tag of the created feature
expTag(Tag): Tag of the created expression
License requirements: None