NXOpen.UF.Gexp.CreateAngle¶
-
Gexp.
CreateAngle
()¶ Refer to UF_GEXP_create_angle for documentation.
Signature:
CreateAngle(fromObject, qualifier1, object1Xform, toObject, qualifier2, object2Xform)
Parameters: - fromObject (Tag) – Tag of object to create the angle from. Valid object types are: UF_line_type, UF_datum_plane_type, UF_datum_axis_type, UF_solid_type. A solid edge should be linear and a solid face should be planar. Occurrence tags are not allowed. Use the prototype tag instead.
- qualifier1 (
NXOpen.UF.Gexp.Qualifier
Refer to UF_GEXP_qualifier_e for documentation.) – Qualifier for object1, only applicable to lines and edges. - object1Xform (Tag) – Tag of transformation for first object. The tag is NULL_TAG if the object is in the same part in which the feature is created.
- toObject (Tag) – Tag of object to create angle from. Valid object types are: UF_line_type, UF_datum_plane_type, UF_datum_axis_type, UF_solid_type. A solid edge should be linear and a solid face should be planar. Occurrence tags are not allowed. Use the prototype tag instead.
- qualifier2 – Qualifier for object2,only applicable to lines and edges.
- object2Xform (Tag) – Tag of transformation for second object. The tag is NULL_TAG if the object is in the same part in which the feature is created.
Returns: A Tuple
Return type: A tuple consisting of (featureTag,expTag)
featureTag(Tag): Tag of the created feature
expTag(Tag): Tag of the created expression
License requirements: None